Coordinaide™—The S&C Protection and Coordination Assistant (v:5.1)

This application runs best under Microsoft® Internet Explorer 7.0 or greater with zoom set to 100%.

Conditions of Use

S&C does not accept responsibility for, nor warrant the proper application of non-S&C protective devices, or the accuracy of their respective time-current characteristic curves. Moreover, S&C is not responsible for any errors, mistakes, or miscalculations that may occur through use of the Coordinaide® application. Results should be reviewed and approved by a consultant or end user who is familiar with the principles of selective coordination and system protection.

This program is the property of S&C Electric Company, Chicago, IL and may not be sold nor may any part of the program source code be used such as to produce a commercial, marketable product.

Minimum Browser Requirements

This application runs best under Microsoft® Internet Explorer 7.0 or greater with zoom set to 100%.

Users Guide

For additional help with Coordinaide, click here.

©2016 S&C Electric Company All rights reserved.

 Coordinaide Software rev:5.1.0 (date:3/26/2016)
Coordinaide Database rev:5.0.0 (date:12/15/2015)